Skip to main content
blog | How to Select a Servo Drive |
|
2 minute read

A servo drive should be selected based on the specific servo motor used in the application. The motion requirements of the driven mechanism determines the voltage and current requirements of the servo motor – the key information required when selecting a servo drive. The motor specification sheet indicates the peak and continuous current requirements along with the motor voltage rating. Since many servo motors have as much as a 4 to 1 peak to continuous rating, careful consideration of the application peak torque requirements is important.

After the motor voltage and current requirements is determined, a drive can then be selected since a servo drive is rated based on its voltage and current capabilities. For a brushless DC servo drive, the input voltage determines the operating DC bus voltage to power the motor. The drive specification will consist of an input voltage and continuous and peak current ratings. It should be noted that most servo drives on the market today have a 2- or 3-times peak to continuous current rating, with the peak current available for short bursts of less than a few seconds.

Example 1
Application requirements led to a selection of a motor with a voltage rating of 240 Vac, a continuous current requirement of 3 amps and a peak current of 5 amps for acceleration. The proper drive for this application would be one with a voltage rating of 240 Vac with a continuous rating of 3 amps. A 3-amp drive will likely have a 6 or 9 amp peak current rating – well within the requirements of the application.

While matching the motor voltage and current requirements will make certain the drive has sufficient operation power, several other servo drive considerations: motion requirements, feedback options, and available communication protocols, will help determine the exact servo drive suitable for the application. Whether the motor will operate in a torque, velocity or position loop will determine the complexity of the servo drive selected. Feedback options are important since a motor may incorporate a specific feedback element that must match the drive’s ability to accept. Finally, a servo drive that is incorporated into a broader automation system may need to communicate on a specific network or fieldbus.

Example 2
A motor requires 240Vac, 8 amps peak for 1.5 seconds, and a continuous rating of 2 amps. For this application, a drive with more than 8 amps would be required to meet the peak requirements. While only 2 amps are needed for continuous operation, a 3 amp continuous drive with a 9 amp peak rating would be required. With an amplifier with a rated continuous current above the motors rating, temperature monitoring would be recommended to help prevent inadvertently overheating the motor.

Selecting a servo drive requires a strong comprehension of motion control systems and the various factors that affect their performance. A motion control expert provides the expertise necessary to navigate the complexities of the selection process. In addition, a good practice is to purchase the drive and the servo motor from the same manufacturer since their ratings are optimized to work efficiently as a system.

Know your current and voltage requirements for a drive? Enter your specifications to search and compare our products, identifying what best fits your needs with our Product Selectors tool.

Consult an Expert

1G Motion System

Discover motion made for your machine. The Kollmorgen 1G Motion System provides a broad range of options, features and confidence to build without compromise.
Learn More

AKD Servo Drive

AKD® Series is a proven perfomer, supporting the largest customer installed base, and offers:

  • Industry leading motion control loops
  • Extensive motor feedback and drive fieldbus support including EtherCAT, EtherNet/IP, Profinet RT, etc.
  • Plug-and-play with Kollmorgen motors
  • WorkBench GUI, acclaimed for customer experience and usability
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Application Example

Learn How to Simplify Motion System Design Across Every Axis and Budget >

| 2:30 PM India Standard Time
Motion system design is becoming increasingly complex, while project timelines and budgets continue to tighten. Machine builders need solutions that help them move from specification to commissioning faster without sacrificing performance,…
English, IN
Lithium Battery Welding Equipment

Linear Motor Functional Safety Advances Safety & Productivity in Lithium Battery Welding Equipment >

Kollmorgen’s SMM functional safety helps achieve stable, controlled motion and global compliance for lithium battery production and competitiveness.
manufaturing facility with multi-axis motion control

Mastering Multi-Axis Motion Control in Modern Production Cells >

When motion systems scale, synchronization gets harder. Learn how modern production cells maintain precision, stability and throughput at speed.
Kollmorgen HV Essentials

Kollmorgen Introduces New Controller and High-Voltage Capability in its Essentials Portfolio >

Kollmorgen Essentials adds a new eight-axis controller and high-voltage drive capability to right-size motion system builds for industrial applications.
Introducing the latest update to SafeMotion monitor firmware - SMM 3

Kollmorgen advances linear motor safety and performance with SafeMotion Monitor firmware upgrade >

The latest SafeMotion Monitor™ firmware (SMM 3.0) expands functional safety for linear motors with EnDat 2.2 safe feedback support and SIL 3 compliance.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…
English, UK
Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español)

Kollmorgen Essentials™: Sistemas de movimiento completos para cada eje y cada presupuesto (Español) >

Descubre cómo Kollmorgen Essentials ofrece control de movimiento de alta precisión y fiabilidad comprobada, ahora más rápido de configurar, más fácil de integrar y más rentable de escalar.
Español
Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever

Off-the-Shelf Motion Powers Fastest Cube-Solving Robot Ever  >

Learn how an off-the-shelf motion system powered the fastest puzzle cube-solving robot. Speed, precision and synchronized multi-axis motion explained.
Kollmorgen Essentials™: Complete Motion Systems for Every Axis, Every Budget

Kollmorgen Essentials: Complete Motion Systems for Every Axis, Every Budget >

Discover how Kollmorgen Essentials delivers high‑precision motion and proven reliability—now faster to specify, simpler to integrate, and more affordable to scale. The new Kollmorgen Essentials line introduces complete, pre-engineered motion control…