Resolution in Position Loop
Valid for S300, S400, S600, S700
Resolution in the position loop must be set precisely for linear applications or gearing with rotary appliaction to get a simple positioning with SI units.
You can setup the resolution with the setup software
- S300/700 screen page Units/Mechanical
- S400/600 screen page Position/ Position Data
Examples for unit selection and resolution related to the application: