Deep water application
Hi,
We are investigating an electric drive for a deep water application (down to 4000m).
A rough specification is as follows:
-
Speed range 0 – 360 rpm
-
Max torque in the range 60 – 80Nm for a period of 1-2 sec.s, then reduced torque in the range 10 – 50Nm for the rest of the duty cycle. Repetitive cycles that last typically 100 sec.s. The drive will be operative for typically 16 hours, then rest for 8 hours and start all over again.
-
Aimed liftetime is 3000 hours.
Question 1:
Will the Goldline servomotor ME-205-A serve this application?
This was the most appropriate motor I could find entering the “Goldline S Series Submersible Servomotors” link.
Question 2:
I have specified an ME rather than a M version, but positioning accuracy is not critical. What is the difference between a framless resolver and a commutation encoder?Question 3:
Are the Goldline servomotors prepared for pressure compensation, i.e. the motors may be filled with thin oil connected to a compensation hose/bellow?
Question 4:
Will flying leads be the best choice for a deep water, pressure compensated motor?
Question 5:
In order to reach the specified speed range and torque, a Goldline P1C gearhead is looked at (reduction ratio 10:1).
Can this gearhead be used for deep water application, i.e be pressure compensated?Question 6:
Will the P1C planetary gearhead fit directly on to the ME-205-A motor, and such that the complete unit (motor + gearhead) can be pressure compensated?
Comments & Answers
Dan.Wolke@Koll… said ...
The Goldline S series is our best motor for your application. We have working applications that far exceed your 4000 meters. Because of the nature of the typical use of this motor, I can't discuss much more details over an open forum. Can you contact Hurley Gill @ [email protected] with more details about what your looking for?