The following chart demonstrates the differences in byte allocation for the command and response assemblies for the AKD1G and AKD2G EtherNet/IP drives.
A subnet mask is a bit mask used to define a subnet of an Ethernet network. It acts like a filter to only allow devices with certain IP addresses to communicate.
Subnets are used to specify which devices can communicate with which other…
This video series comprises of 16 videos as a complete training on AKD Ethernet IP Communications. Videos 1 though 7 are essential and the remaining videos can be viewed in order or the user can pick and choose a topic of interest or one that…
This article demonstrates potential issues seen when users attempt to import the data types that the AOIs are codependent on and how to resolve them.
This applies to the use of the AKD-P EtherNet/IP motion tasking drive ( AKD-P-NxEI ) and the…