This PowerPoint presentation explains the differences between different types of servo motor feedback devices, including:
The differences between absolute and incremental devices.
The differences between analog and digital devices.
Typical…
First to review what F402 means:
Analog signal amplitude for resolver or sine encoder feedback is out of range, either too low or too high.
To troubleshoot:
Check primary feedback (X10 connection), for resolver and sine/cos encoder only.
The setting for FB1.ENCRES (Rotary Encoder Resolution) for a resolver is set automatically in Workbench to a value of 32768 * FB1.POLES. So it is set to 65536 for a 2-pole resolver or 131072 for a 4-pole resolver. A resolver does not have…