Some users have reported display issues within WorkBench, the symptoms usually are cut texts or images, missing elements or missplaced elements.
Issue:
The problem is due to the fact that part of our application is working using WinForms technology…
Choosing a controller that matches your project is important. You don't want to overspend on a device that is significantly more powerful than you need, but buying something that is not robust enough can be even more costly. By defining your…
Os servo-motores são controlados por drives que utilizam um método chamado de malha de controle. A malha executa um cálculo com a realimentação da posição do motor e o valor de comando, visando reduzir ao máximo o erro através do ajuste dos…
PxMM project variables can be read directly from the Internet Explorer (IE) web browser.
Syntax and Examples
The syntax for a global variable is:
http://10.8.41.40/kas//plcvariables?variables=ActPos1
The syntax for…
The KASIface application is to show how a KAS-variable access can be implemented into a mobile device. This example uses http request in the text format. The programming is done with Java in Android Studio.
Firefox offers a utility HttpRequester to read/write information in its web browser through HTTP communications. The tool can be useful to a KAS user who want to become more familiar with PxMM HTTP communication
A beta version of the KAS Webhelp is available from the landing page of KDN (see "Resources" in the right column) and from the following link. This version includes additions and corrections made since the last official software release. This help…