The AKD command source (DRV.CMDSOURCE) is set automatically by the EtherCAT/CANopen master controller. There is no need to set this in Workbench when using the fieldbus. And there is no need to read DRV.CMDSOURCE to verify that it's set…
I'm using an AKD-P01206-NBCC drive via CANopen.
In profile position mode, I'm commanding the drive to various positions, and then
watching the "Target Reached" bit of the status word to see when the drive gets there.
A problem occurs when the…
Help setup the AKD2G in DS402 Profile Velocity mode.
This document assumes the EtherCAT Master has “free mapping” function available. The ability to select what data is to be shard every update cycle. This information may not make sense to you…