The DDL catalog shows a dynamic bend radius of 15X the cable diameter for the MxC, TxC, HxC cables. The static bend radius for these cables would be 10X the cable diameter. It is important note as stated in the DDL catalog, the…
Two Motors Can Be Mechanically Connected to a single Drive
In this example DDL motors are used. However, linear, rotary, and permanent magnet motors also apply.