In October 2016, an inter-compatibility test was performed together with the company Heidenhain. In this event, the AKD was tested successfully with various types of Heidenhain Endat 2.2 encoders.
The devices tested can be found in this…
This question comes up quite a bit about the Heidenhain Endat . Saying Endat 2.2 is only half the story. There is Endat 2.2/01 which is the analog version. Endat 2.2/22 is the fully digital version. Endat 2.2/01 and…