Skip to main content

Kollmorgen Support Network

AKD2G - Sending Secondary Feedback through EtherCAT >

The AKD2G's various feedback options allow for incorporating up to 5 feedback devices into the drive. Occasionally the feedback is not used for servo AXIS control (a position used as a direct command or feedback to a servo axis) but used as an…

Linear Encoder Supported by AKD, S700, and S300 >

List of known linear encoder supported by AKD / S700 / S300.
Subscribe to Linear Encoder