Hello community,
We have a AKM23D motor. We are monitoring the +-24V brake signal, which seems to have a lot of noise and we think that this could be the cause of a random stop of the motor.
As you can see in the following figure, the stop of…
We are using a servomotor type AKM42E for acoustic measurements in anechoic chamber.
It would be useful to know the type of the bearings mounted in such a servomotor. The idea is to know the following data to recognize some features in the…