Skip to main content

Kollmorgen Support Network

Establishing Commutation for Encoder-Halls Based Motors with the AKD/AKD2G >

Commutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases.  If the rotor position of the motor is not determined correctly or the…

Establishing Commutation for Resolver Based Motors with the AKD/AKD2G >

Commutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases.  If the rotor position of the motor is not determined correctly or the…
Subscribe to phasing