Profibus Option Card Labels:
The Profibus option card for the S300 and S700 is labeled "Proibus DP". (OPTION = H0Cxx)
The Profibus option card for the S600 is labeled "Profibus". (OPTION = H02xx)
The two option…
There is an undocumented parameter in the S300, SOFTIN. Bit 0 of this variable is for input 5, bit 1 for input 6,..., . If you set SOFTIN = 1, IN5 will return 1.To operate the brake set IN5MODE = 32.With SOFTIN = 1 the (virtual) input 5 is…
Profibus Communication Rate and Bandwidth
The update rate of the Profibus communications is set in the Profibus master controller. The GSD file of the drive allows a minimum time of 2ms.
The Profibus master will send the complete…
Multi-Fieldbus is the ability of Kollmorgen servo amplifiers to communicate with a lot of different fieldbus systems. These bus systems are accessible either with option cards, firmware variants or device variants.
Valid for S300, S400, S600, S700
The Profibus protocol does not give any support for synchronizing the start of motion tasks. To start several drives synchronized, it can be useful to define the motion tasks by fieldbus but start them via a…