Skip to main content

Kollmorgen Support Network

What is the best approach to read a pulse signal from a speed sensor with AKD BASIC Drive, X7 (DIN1) or X9 connector?  >

I am having a hard time of reading an accurate speed on the AKD Basic Drive. Some background information is I have a 48Vdc clutch coupled to KBMS 48Vdc motor. Operation mode is when clutch speed hits a target speed, motor comes on and when motor…

VUNIT Parameter (S300-S700) >

ASCII - Command VUNIT    
Subscribe to Speed Resolution