Skip to main content
Success Story | 2 minute read

Transbotics

A GLOBAL PRIMARY METAL MANUFACTURER USES AGVS TO MOVE HEAVY LOADS IN A HIGH TEMPERATURE ENVIRONMENT

An international primary metal manufacturer uses Automated Guided Vehicles (AGVs) in a new plant to move heavy loads in a high temperature environment. The AGVs were implemented to provide reliable transportations and to minimize damage to the load. The customer was so pleased with the benefits of the AGV system that they have implemented the solution in multiple plants around the world.

Transbotics, a global channel partner to Kollmorgen, has implemented an AGV system based on Kollmorgen’s AGV control technology in a new plant for an international primary metal manufacturer. The customer needed a cost-effective solution capable of consistently moving coils and work rolls through the production process. One challenge was the different shape of the load and its extreme temperature. The 20 ton coils varied substantially in size compared to the work rolls and the surface temperature could well exceed 150 C˚ (~ 300 F˚). Adding to the challenge was meeting the speed requirement while keeping the load stable and transportation reliable. “The customer’s primary concern was the movement of extremely hot, large loads reliably and without damaging a pliable load”, explains Jayesh Mehta, Marketing & Aftermarket Sales at Transbotics.

Transbotics used Kollmorgen components designed for rough environments to provide a heavy-load laser guided vehicle for the application. Kollmorgen’s laser navigation platform is already successfully guiding well over 10,000 AGVs. Kollmorgen’s AGV control solution promises lower total costs for system integrators and end-users. It is applications-independent and scalable, from the small and simple to the big and complex. The control solutions are applied in more than 17,000 AGVs around the globe. The benefits of the AGV system were immediately recognized. The fast Return-On Investment (ROI) of the AGV system and the reliable transportations day after day were so appreciated by the customer that they have implemented the solution in multiple plants around the world.

AGV Systems

Our NDC8 platform is a complete, general-purpose control solution for automatic forklifts and other AGVs. This application-independent, scalable solution is easy to integrate with existing vehicle designs as well as host systems and material handling solutions.

Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Accelerate Your AGV Expertise with Kollmorgen's Comprehensive Training Program

Accelerate Your AGV Expertise with Kollmorgen's Comprehensive Training Program >

In today's rapidly evolving world of automated guided vehicle (AGV) systems, staying ahead of the competition requires continuous learning and skill development.
ChatGPT, Google Bard or Microsoft CoPilot and AGVs: Balancing the Benefits and Challenges

ChatGPT, Google Bard or Microsoft CoPilot and AGVs: Balancing the Benefits and Challenges >

Could prompt AI such as ChatGPT, Google Bard or Microsoft CoPilot revolutionize the AGV arena? Sebastian Witkarsson, Information Security Officer at Kollmorgen, examines the possibilities – and sounds a note of caution.
Unlock fast-track AGV commissioning with Cirrus

Unlock fast-track AGV commissioning with Cirrus – the latest innovation from Kollmorgen >

Cirrus, the latest commissioning innovation from Kollmorgen, is a cloud-based solution that speeds up and streamlines AGV installations. With its smart features and easy-to-use interface, Cirrus can help accelerate your business by enabling efficient…
Kollmorgen Innovation Day, Realizing Ideas at the Cutting Edge of Tech

Realizing Ideas at the Cutting Edge of Tech >

Kollmorgen is all about innovation, constantly investing in collaborations and research projects to exchange knowledge and expertise with partners and universities across the world. Learn more about how Kollmorgen works to enable innovative thinking…
NDC Solutions, Kollmorgen, Yeefung

AGV car parking robots >

Yeefung, an AGV partner to Kollmorgen, has developed a new generation of their car parking robot.
Kollmorgen NDCSolutions, Arla Foods in Götene, Sweden

Arla Foods in Götene, Sweden >

Arla Foods uses an AGV system that has expanded over time in a dairy warehouse.
Kollmorgen NDCSolutions, Borealis

Borealis >

Borealis uses AGVs to minimize operational cost and damage to goods.
Kollmorgen NDCSolutions, System Group

System Group >

The collaboration between Kollmorgen and Gruppo System Spa resulted in the creation of an AGV vehicle which was 100% customized for a “big player” in the automotive sector.
Kollmorgen NDCSolutions, Bring Logistics

Bring Logistics >

Bring Logistics minimizes operational costs with automated VNA trucks.