Effective treatment of disease begins with fast, accurate diagnosis.
In vitro studies of patient fluids, cells and tissues influence 60% to 70% of clinical decisions.1 Even before the COVID-19 crisis arrived, new test methods and growing test volumes were already driving a strong need for new and upgraded clinical analyzers—both in the laboratory and at medical centers. Maximum productivity requires quick, precise, coordinated motion for positioning pipettes, aspirating aliquots, dispensing reagents and more.
As a trusted supplier to many major manufacturers, Kollmorgen understands the specialized motion requirements of in vitro diagnostic devices.
Kollmorgen motion systems offer precise single-axis or coordinated multi-axis control. Our broad portfolio includes compact designs that provide the torque and power density needed for highly dynamic motion even in a small machine footprint or in low-voltage/mobile applications. Our Powermax NEMA 23 stepper motors deliver precise motion control without the need for encoders and feedback circuits, and they feature oversized bearings for increased service life.
With these and other motion products, we offer an extensive selection of standard models and rapid prototyping of customized options for a perfect fit.
Top Products for In Vitro Diagnostics
![](/sites/default/files/styles/webp_conversion/public/AKM_Series_MEDIUM_2_2.png.webp?itok=jcn_rnI0)
AKM Motors >
Our best-in-class, high-performance servomotors offer a wide range of mounting, connectivity, feedback and other options. More than 500,000 standard models are available along with co-engineered modifications to suit almost any application…Related Resources
![Rapid Scale-Up of Blood Gas Analyzer Production, Kollmorgen Rapid Scale-Up of Blood Gas Analyzer Production, Kollmorgen](/sites/default/files/kollmorgen-case-study-blood-gas-analyzer.jpg)
Rapid Scale-Up of Blood Gas Analyzer Production >
The COVID-19 pandemic has created a massive spike in the demand for medical equipment in every region of the world, including personal protective equipment, laboratory test systems, ventilators and more. A major global supplier of blood gas analyzers…![Rapidly Scaling Production of Critical Equipment, Kollmorgen Rapidly Scaling Production of Critical Equipment, Kollmorgen](/sites/default/files/kollmorgen-face-mask-case-study.png)
Rapidly Scaling Production of Critical Equipment >
In the fight against COVID-19, the soaring demand for face masks has led to a severe undersupply. Beckmann Automation GmbH, a German machine builder that has traditionally manufactured machines for mattress and belt production, quickly stepped…![Kollmorgen Helps Rapidly Scale CT Scanner Production, Kollmorgen Kollmorgen Helps Rapidly Scale CT Scanner Production, Kollmorgen](/sites/default/files/kollmorgen-case-study-ct-scanner.jpg)