Getting Started with PxMM UDP Communications - using Packet Sender
KAS UDP Communication
Introduction
This application note uses the PC utility Packet Sender (download at https://packetsender.com/) to perform simple communications between a PxMM and a PC. The program “udpProgram” in the project UDP test Send-Receive First Transmission Each Way.kas has been added to a .kas starter project (attached).
IP Addresses
- PC address:192.168.0.100
- PDMM Address: 192.168.0.102
Note: You may need to use different IP Addresses that fits with your network addressing scheme.
PDMM to PC communications – key function blocks
Setup
- Sending PDMM’s Port Number: 10 (using udpCreate and create the Socket to send Data)
- Receiving Device’s Port Number: 20 (using udpAddrMake )
- Receiving Device’s IP address: 192.168.0.100 (using udpAddrMake )
- Command to Send Data: udpSendTo
PC to PDMM communications – key function blocks
Setup
- Receiving PDMM’s Port Number: 50 (using udpCreate and Create the Socket to Receive Data )
- Command to Receive Data: udpReceiveFrom
Port Summary
Product | Port Number to Receive Data | Port Number to Send Data |
---|---|---|
PDMM | 50 | 10 |
PC (Host) | 20 | xxxx |
Operation
- Startup UDP Sender on PC
- Go to File / Settings then Network Tab and setup as follows
and setup as follows:
- In the Packet Sender main screen setup as follows:
- Startup PxMM Project
- First PxMM Transmission: In the IDE Dictionary set StartTest = 1 to start the test. See that the following line has been Added to the Packet Sender Log
- First PxMM Transmission: Observe the following log entry has been added:
- First PC Transmission: In Packet Sender Click on the Send Button
- First PC Transmission: Observe the following log entry has been added:
- Complete log: