Skip to main content

 The Difference Between Continuous Ratings and Holding Continuous Loads

This white paper explores AC servo motor sizing considerations and the often-resulting miscommunication issues that may arise for an application that must continuously hold a load with little movement. We’ll provide an in-depth explanation of the often-misunderstood term “stall” as it is typically used in the servo motor industry, then apply this information to calculate the axis’s effective RMS force/torque to achieve correct motor sizing.

Fill out this short form

to view this White Paper

-OR-

Login / Register

to gain access to Kollmorgen content

Privacy Statement - By sending us your contact details you agree that your personal data/user behavior can be electronically stored and processed. If you no longer wish to receive the enewsletter, you can unsubscribe at any time.

CAPTCHA

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure washdowns are essential to keep machines free from pathogens, yet these washdowns are often incomplete, ineffective and damaging to motors and other equipment. Common practices such as shielding or bagging motors to prevent damage are extremely time-consuming. Direct washdown of equipment that is not properly designed to prevent water ingress can lead to premature failure. Irregular and rough surfaces can harbor pathogens that are difficult to remove. Eliminate all these issues by employing these best practices for the design of a more hygienic and productive machine.
Learn More

AKMA Servo Motors

The lightweight AKMA servo motor is designed for harsh environments like food and beverage processing, and delivers performance and reliability.
Learn More

Engineer the Exceptional

Learn how to engineer exceptional machines, robots and vehicles with the highest-performing, most reliable motors, drives, automation solutions and more.

Learn More

Related Resources

Easy-to-Clean, Durable Motion Systems for Food Processing and Packaging >

The food processing and packaging industry plays a major role in ensuring that the final product is safe to consume. While food safety is a serious requirement, it also presents significant challenges for manufacturers. Frequent, high-pressure…

Clean and Productive — Improving Food Safety and Packaging Machine Reliability  >

Clean and Productive — Improving Food Safety and Packaging Machine Reliability: Learn how food processing and packaging machines can endure direct washdown without the risk of damage to motion systems. Meet food safety requirements while maximizing…

Accelerating the Development of Next-Generation Prostheses and Exoskeletons >

Learn how Kollmorgen servo technology is helping OEMs accelerate the design of next-generation prostheses and exoskeletons.

Kollmorgen and Stereotaxis Advance the Precision and Safety of Surgical Robots >

Kollmorgen’s advanced motion products and expertise are helping save and improve lives. Learn how the new Genesis surgical robot incorporates torque-dense AKM servo motors with specialized, integrated encoders to revolutionize cardiac ablation…
Kollmorgen Express Delivery significantly shortens lead times for the company’s most popular motion products

Kollmorgen Express Delivery significantly shortens lead times for the company’s most popular motion products >

Motion leader Kollmorgen announces a new classification for select products that can be delivered within an accelerated timeframe.

From the Factory to the Farm: Unleashing the Power of Kollmorgen's Servo Motor Technology >

As smart automation increases farm productivity, there is a need for powerful, precise motors that can handle a wide range of heavy-duty tasks, day in and day out. But even the most advanced technology doesn’t change the basic nature of farming.
Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats

Kollmorgen’s low-temperature servo technology simplifies cleaning of solar energy heliostats >

The development of photovoltaic and thermal solar energy—along with China’s rapidly growing capacity to manufacture them—has opened many new opportunities for sustainable energy production in international markets. At the same time, the demand for…

VLM Motor Selection Guide >

Selection guide for the discontinued VLM servo motors

Stop, hold and go safely: Motion tuning for vertical loads >

When designing motion for applications such as vertical gantries and hoists, you need to take special care to ensure operator safety and operational efficiency. Let’s discuss best practices for meeting the particular challenges involved.