Introduction
Taking a look at PLC projects, we see that every machine deals with the same functionalities. Generally, machines powered by servo drives, need to follow a sequence of steps during its development:
…
We are often asked if an AKD-P-NBEI ( EtherNet/IP ) drive can use step/dir (electronic gearing ) or analog as the command source and simply use EtherNet/IP for
basic functionality like enable/disable, fault reset, and diagnostics.
Article https://kdn.kollmorgen.com/content/scaling-2nd-feedback-kas-ide covers encoders with the following formats:
This article covers the differences when setting up an Endat 2.2…
This article outlines setting up a digitizing axis (secondary external encoder) or encoder master in a PxMM controller application that is using the PLCopen motion engine. The encoder input port is: AKD connector X9.
Acceptable formats for the…
Valid for S400, S600 with FW 6.21...6.99
With operation mode 4 (OPMODE 4, electronic gearing) the axis follows synchronously to a master position. The gearing ratio can be adjusted with GEARI and GEARO.