General
The servo amplifiers S300, S600 and S700 have an expansion card slot. The servo amplifier's Instruction Manual describes how to install the expansion card to the slot.
The option FAN Option (S700: F2, S600:FAN) is an electronics, which controls the velocity of the integrated fan depending on temperature measurement. This reduces the overall noise emission of the servo amplifier. The servo amplifiers must be ordered…
Industrial use of ever-faster and technically more complex servo drives in all areas of machinery, plant and equipment manufacture requires high-quality accessories.
No EMC problems, safe drive operation, Plug-and-Play are guaranteed with the…
Profibus Option Card Labels:
The Profibus option card for the S300 and S700 is labeled "Proibus DP". (OPTION = H0Cxx)
The Profibus option card for the S600 is labeled "Profibus". (OPTION = H02xx)
The two option…
This excel file contains many of the accessories sold in the U.S. and Europe. Often the U.S. part number will coincide with the European standard of DE-XXXXX. This file contains the part numbers that diverge from this standard.