The Servostar S300, S600, and S700 drives have a digital input mode called Command Buffer. This mode allows ASCII commands to be run in a sequence when the input goes high and low. But in order to make sure the commands are…
For the S300, what is the resolution of the trigger point to turn outputs on based on a < or > of actual current? This would relate to I<actO1TRIG and I>actO1TRIG in O1MODE=8 or O1MODE=9. The internal current resolution is depends…
Valid for S600 with Firmware 588dpr174u only
With varying loads coupled to the motor the parameters GV and GP can be switched over very fast by using edge control of digital input 2 and the ASCII command VAR..
The command VAR is used only…