The detailed requirements for each release are indicated in the release notes. In this article, we list the different versions in which the minimum requirements have changed.
All Kollmorgen PMDC (Permanent Magnet DC) motors are good for continuous operation from -20 degrees C to 40 degrees C. If the requirement is for temperatures below this, we can go to -40 C with a bearing grease change. On the…
Over the years, Kollmorgen has offered 120V/230V drives that can operate on a single phase AC supply. Most of these are for laboratory or college applications. In some cases, these applications experience under voltage faults or…