The AKT2G family is recommended for new applications requiring remote I/O in a PCMM or PDMM KAS application. This article and attachment compares the AKT2G Remote I/O family with the AKT Remote I/O family.
This PowerPoint presentation explains the differences between different types of servo motor feedback devices, including:
The differences between absolute and incremental devices.
The differences between analog and digital devices.
Typical…
Following are the instructions for adding the Encoder 802-004, which is the 0.25" SHAFT, 500 LINE ENCODER for stepper motors. Attached is the original PDF.
NOTE: S3 & S4 motors require cover mod. for cable
General Information
The LDA…