Attached is the letter of compliance for All Standard Catalog AKIM Models represented by AKM1, AKM2, AKM3, AKM4, AKM5, and AKM7 comply to DIRECTIVE 2011/65/EU.
An AKM motor with resolver can be operated with an SC900 series amplifier providing that the motor is within the current limitations of the drive. Typically the motor resolver offset must be set to 240. This is in the configuration screen and called…
General
Cogging torque designates a phenomenon with electrical motors, which possess permanent magnets in the stator and a slotted anchor from electric sheets or a slotted stand and an anchor with permanent magnets.
The servo motor is an engine, that can drive to different set point positions and then maintains these in the sense of a control drive. The position is thereby in case of a rotatory engine a angle position and in the case of a linear motor a…