The AKD command source (DRV.CMDSOURCE) is set automatically by the EtherCAT/CANopen master controller. There is no need to set this in Workbench when using the fieldbus. And there is no need to read DRV.CMDSOURCE to verify that it's set…
DeviceNet is a CAN based field bus which is used mainly in the automation engineering.
Number of nodes
Maximum 64 nodes per bus segment. Node addresses (0 to 63) can be set with DIP switches on the servo amplifiers.
Baudrate
Selectable…