Workbench throw an exception when compiling basic code.
I just can't work !
I can connect to the real AKD and control it but no way to compile any code.
I tried to create an empty project with a simulated AKD-BASIC and compile an empty code file…
A crash can occur when creating a new project and there is no default printer selected on the PC. The workaround is to set a default printer. Here is the procedure for selecting a default printer:
1. Click on the Start button and type…
Several crashes of the KAS IDE have been traced back to a faulty graphics driver on the host PC. The crash happens when opening any KAS project.
The only way to determine if the crash is due to the graphics driver is to analyze the crash dump file.…