Why use motor chokes? The motor choke: compensates high capacitive charge/discharge currents typical of shielded motor cables approx. 25 m and longer; reduces current alternation noise in the motor; reduces current ripple in the motor. Read more.
The attached demo project shows how to control a servo axis with a KAS controller in Torque Mode instead fo the default Position Mode. This project requires a 2.9 release of KAS software and PDMM firmware, which is currently only available in beta…