Skip to main content

Kollmorgen Support Network

Wiring of KCM with High EMC Requirements >

In cases where the cable length is  >500mm or there are high level EMC requirements, observe the notes given below. Connection Use a shielded cable for DC-Bus link connection. The shield should be connected on both ends. The wires for…
Subscribe to dc-bus