Important to note is that the Import Project feature in KVB is for Exter panel based Information Designer project migration to KVB. If the HMI project was done with Cimrex panels the migration is two stepped where you need to first update the…
This article refers to G&L PiC application note and provides a step by step example to establish communications between an Exter Terminal and a Digital MMC. For more information, download document AN000055.