How To Guide for Migrating from Old Exter/Cimrex panels with G&L drive resident control to KVB.
Important to note is that the Import Project feature in KVB is for Exter panel based Information Designer project migration to KVB. If the HMI project was done with Cimrex panels the migration is two stepped where you need to first update the Cimrex Prog project to Information Designer and then next to KVB.
Also remember that the migration is 85-100% complete and the project may need some tweaking because some features in the older units/SW (dynamic display, scripting, etc.) are no longer supported in KVB.