In cases where the cable length is >500mm or there are high level EMC requirements, observe the notes given below.
Connection
Use a shielded cable for DC-Bus link connection. The shield should be connected on both ends. The wires for…
If you suspect that you're experiencing EMC issues, this is a method used to identify intermittent communication failures on Hiperface DSL®.
Step 1 - Enable the Counter
The first thing to do is to enable logging certain events within the Workbench…