A recipe can be used in an HMI program to store and select groups of data to be used without having to enter the data each time it is used. It is easy to create a recipe in KVB by clicking on Insert / Recipe and give the recipe a name.
A…
Attached is a demo program that contains two subprograms to import data from a file on a PDMM SD card, or export data from an array to the SD card. This data can then be used to build a cam profile in the program and update the motion on the…
The term "dual use" identifies the basic usability of a technology (both a machines and software) as used for both peaceful and military purposes.
For example, drive components used in high-speed centrifuges can be used in both pharmacology and for…
Valid for S300, S700
Most of the ACOMEL drives used in high frequency applications can be replaced with S300/S700 servo amplifiers with special firmware.
Dual Use
These devices are export controlled ( Dual Use, AL-3A225 ) and require an export…