Export Classification
Applicable for ServoStar drives S300, S400, S600, S700
The firmware installed in the servo amplifier defines the export classification of the device (No 3A225 of Appendix I of (EG) No. 428/2009). Servo amplifiers, which are not affected by the Dual Use directive, include a limitative firmware (frequency range below 600 Hz). This firmware ist signed with the extension "_ND0". Export controlled firmware cannot be uploaded to non export controlled amplifiers, see also Warnings and Fault Messages, message"DUF".
All servo amplifiers with firmware, which does not show the extension "_ND0", are export controlled.
Contact Kollmorgen Europe GmbH if you need replacement for export controlled Firmware.
KOLLMORGEN Europe GmbH
Pempelfurtstraße 1
D-40880 Ratingen
Germany
Tel: 0049 (0) 2102 9394 0
Email: Vertrieb (Sales) [email protected]
Email: Support [email protected]
Amtsgericht Düsseldorf, HRB 35844
Geschäftsführer:
Dennis Gallagher, Guido Reinke, Colin Davis
EG-IDNr.: DE813835822