In cases where the cable length is >500mm or there are high level EMC requirements, observe the notes given below.
Connection
Use a shielded cable for DC-Bus link connection. The shield should be connected on both ends. The wires for…
This article describes how to remove the outer cable jacket from the AKMH motor cable and solidly clamp it to the servo drive’s grounding bracket. For more information, see the application note: AKMH Cable Modification Application Note