Article https://kdn.kollmorgen.com/content/scaling-2nd-feedback-kas-ide covers encoders with the following formats:
This article covers the differences when setting up an Endat 2.2…
If two or more PCMM networks have to follow the same position set point, it's possible to use the following strategy.
The image below shows a typical configuration where all the AKD drives must follow the same position set point:
Orange…
This article outlines setting up a digitizing axis (secondary external encoder) or encoder master in a PxMM controller application that is using the PLCopen motion engine. The encoder input port is: AKD connector X9.
Acceptable formats for the…