HIPERFACE® DSL (Sick AG) is equivalent to the two-wire RS485 standard with a transmission rate of 9.375 MBaud. The data transmission is synchron to the servo amplifier clock, which can be up to 11.95 microseconds short.
HIPERFACE®
The High Performance Interface is the standard interface for SICK-STEGMANN motor feedback systems.This interface was specially developed for the requirements of digital drive control and offers the user standardised and…