Commutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases. If the rotor position of the motor is not determined correctly or the…
Commutation is the means by which a servo drive controls the torque of a motor by determining the position of the motor and applying current to the appropriate motor phases. If the rotor position of the motor is not determined correctly or the…
Is it intended behaviour that motor phase, as determined by Wake-And-Shake (WAS), is not saved when the motor drive is turned off?
I am working with a set of three AKM43K-ACC2C-00 motors, controlled by AKD-P02406-NBEC-0000 drives, firmware…
Application Note: Motor-Phasing/wiring: non-standard, S300 or S700 - positive feedback count with a CW rotation as viewed from the lead exit end, for KBM(s) motor.