Skip to main content

Kollmorgen Support Network

Max. Torque in Velocity mode >

Hello, I have the following situation. A Servodrive is connected with CANbus to the controller, the drive is connected to a motor which that drives a belt. Now I want to set the speed and max. torque that of the motor during operation. What is…

Bode Plot Functions >

Valid for S300, S700
Subscribe to speed control