Skip to main content

Kollmorgen Support Network

Encoder Installation Instruction for IDC Stepper Motor 802-004 >

Following are the instructions for adding the Encoder 802-004, which is the 0.25" SHAFT, 500 LINE ENCODER for stepper motors. Attached is the original PDF.  NOTE: S3 & S4 motors require cover mod. for cable General Information The LDA…

Pinout for (IDC) Stepper motors with quick disconnect >

Pin 1 (B+): Red/White (or White) Pin 2 (A+): Red Pin 3 (Ground): Green (or Green/Yellow) Pin 4 (A-): Red/Yellow or Red/Orange (or Purple) Pin 5 (B-): Red/Black (or Black) In some cases, the stripes on the wires are not clearly visible. Check the…

Instructions for Selecting a Stepper Motor >

The Basics of Selecting a Stepper Motor The vast majority of stepper applications are fairly simple in terms of selecting the motor and drive.  Most applications have one or more of a few criteria, usually including torque, speed,…

Pull-In and Pull-Out Torque  >

Some of the stepper motor nomenclature includes some terms not often used today.  Such terms are Pull-in Torque and Pull-out Torque.The information below may be helpful in understanding the different torque values for stepper motors.
Subscribe to stepper motor