Hi,
I use a servomotor type AKM42E coupled with software Drive, for running a fan rotor.
I need to know the absorbed power or the torque of the motor during the operation. It is possible?
Thank you
The PxMM can control the AKD drive in Position, Velocity, or Torque OpMode. The default AKD Drive OpMode in a KAS program is Interpolated Position Mode. This is AKD Opmode 2 as shown on the drive's front LED Display. To precisely control motor…
Hi, I need to know the actual torque value of my a C062C servo motor, so i used the following commands:
A:=MLAxisRateTq(PipeNetwork.Axis2, LREAL#121.6875);
B:=MLAxisReadTq(PipeNetwork.Axis2);
Where the value of 121.6875 is calculate with…
The attached demo project shows how to control a servo axis with a KAS controller in Torque Mode instead fo the default Position Mode. This project requires a 2.9 release of KAS software and PDMM firmware, which is currently only available in beta…