New Features
Next Generation Controller Software
Compatible with PCMM/PDMM (1st Generation Controllers)
64-bit Runtime (2nd Generation Controllers)
AKD2G Modular Device Profile (MDP) I/O
MDP IO support for model variants
New…
New Features
Modular EtherCAT Topology
AKT2G-BRC-000-000 - Brake chopper terminal
Modify PLCopen axis user units from a program
IDE Improvements
For more details, please see the attached release note.
Some users have reported display issues within WorkBench, the symptoms usually are cut texts or images, missing elements or missplaced elements.
Issue:
The problem is due to the fact that part of our application is working using WinForms technology…
Is it intended behaviour that motor phase, as determined by Wake-And-Shake (WAS), is not saved when the motor drive is turned off?
I am working with a set of three AKM43K-ACC2C-00 motors, controlled by AKD-P02406-NBEC-0000 drives, firmware…
New Features
Kollmorgen E-Bus Stepper Integration:
AKT2G-SM-L50-000 - Stepper motor terminal with incremental encoder, 50 V DC, 5 A (Imax), 2 phases
AKT2G-SM-L15-000 - Stepper motor terminal with incremental encoder, 24 V DC, 1.5 A (Imax), 2…
Workbench throw an exception when compiling basic code.
I just can't work !
I can connect to the real AKD and control it but no way to compile any code.
I tried to create an empty project with a simulated AKD-BASIC and compile an empty code file…
New features include TCP/IP Function Blocks, BBH FSoE Master + SafePLC with KAS-IDE and AKD2G w/ SMM, KAS IDE-WorkBench Improvements, new File Management functions, DriveParamStrRead, Multi-select PDO objects, new axis parameter to read PLCopen…
WorkBench (version ≥ 2.2.2.4811) has some accessible parameters to tweak the way data are exchanged with the drive. Keywords sent to the drive and answers returned will be grouped together to build bigger packets of data. This is particularly…