Skip to main content

Kollmorgen Support Network

Test Pulse | 14 Aug 2014 | |

Test Pulse

Valid for S300, S700, AKD

Test pulses are used e.g. by safety controls, function diagnostic devices and EMC simulators for proofing several properties.

Test pulses given to the STO-Enable input, which do not exceed the given length and off-time, will not have any influence to the safety relevant STO function of the servo amplifiers:

image

Pulses with T1 < 300µs and T2 > 200ms will not have any influence to the STO function.