The controlled motion of any given axis of a machine will require the AC mains to be dropped after completion of an emergency-stop (NEC - Category 1). The necessary NEC stop category is determined based on the machine builder’s safety…
This article contains 2 videos and presents sample code for a KAS Safety application with:
SCU Safety PLC with SafePLC2 software (safety parameters defined with SafePLC2 software)
PCMM Machine/Motion Controller
AKD2G Servo Drive with…
New Features
Modular EtherCAT Topology
AKT2G-BRC-000-000 - Brake chopper terminal
Modify PLCopen axis user units from a program
IDE Improvements
For more details, please see the attached release note.
The below video demonstrates how an EtherCAT network can be created with the KAS IDE software and the FSoE parameters can be automatically shared with a BBH Safety Controller. Also, Safety Risk Assessment (SRA) parameters setup in the AKD2G…
This article shows how to make a simple safety Application with KAS and SafePLC2.
The Functional Safety parameters can be configured in WorkBench or in the BBH SafePLC2. Both methods are described here.
This sample configuration illustrates setting up a dual-axis AKD2G with dual-axis KSM 12-2 Safety PLC.
Safety Engineering is not so simple that one design will meet SIL2 for all applications. The intent of this document is to give a…
New features include TCP/IP Function Blocks, BBH FSoE Master + SafePLC with KAS-IDE and AKD2G w/ SMM, KAS IDE-WorkBench Improvements, new File Management functions, DriveParamStrRead, Multi-select PDO objects, new axis parameter to read PLCopen…