New Features
AKD2G Drive Integration:
Single and Multi-Axis drive variants
Features not yet available: firmware download, capture, I/O, feedback #2-5
Note: Please contact Kollmorgen for latest AKD2G firmware and KAS software.
New PCMM…
The AKD2G drives with firmware versions 02-12-00-001 (and later) do not support downgrading the firmware to the versions 02-12-00-000 (or earlier).
The KAS EtherCAT backups created using AKD2G firmware 02-12-00-000 (or earlier) are not capable of…
The S200 updated boards use a larger FPGA with multiple feedback and filter options. Two new parameters have been introduced to select/set these options. These parameters allow the updated boards to use a single FPGA control logic release (LogicVer =…
New Features
Modular EtherCAT Topology
AKT2G-BRC-000-000 - Brake chopper terminal
Modify PLCopen axis user units from a program
IDE Improvements
For more details, please see the attached release note.
New features include:
Enhanced AKD2G Drive Integration
Map EtherCAT feedback to PLCopen Digitizing Axis
Multiple IDE Instances
IDE Ease-of-Use Enhancements:
Elastic Search capability in On-Line help
See the article for more information.
Important to note is that the Import Project feature in KVB is for Exter panel based Information Designer project migration to KVB. If the HMI project was done with Cimrex panels the migration is two stepped where you need to first update the…