We have enhanced our new firmware 6.05 for S700 and S300 to now support the latest AKM2G servo motor family via plug and play. The motor database in the servo amplifier and in the DriveGUI now support AKM2G.
For space reasons, however, we had to…
New Features
AKD2G Drive Integration:
Single and Multi-Axis drive variants
Firmware download
Digital and Analog I/O
Features not yet available: Capture, Feedback #2-5, Backup/Restore
Note: Please contact Kollmorgen for latest AKD2G…
This article will help you understand the differences between older S700 (S701-724) drives with single-channel STO and newer dual-channel STO S700 drives.
The PCMM (Programmable Controller Multi-Axis Master) Dual-Core is a PCMM 1.2GHz with two CPU cores. It shares the same electronic hardware, connectors, and signals as the PCMM single core model. It has the same features, functionality, memory, and…
New Features
EtherCAT Diagnostics with:
Web-server tab with network topology
Functions/FBs for application program
Configurable Working Counter limit in the IDE
New HMIs: X2 Panel Models
New KVB v2.20 software
New function:…
You have just received new KAS installation files consist of KAS IDE installer and PxMM Controller FW. Follow the steps below to upgrade your KAS System to the newer version.
The software for downloading firmware to the Servostar CD series drives is called "Ignite."
The drive must be put into "Ember mode" prior to downloading the firmware into the drive.