I have servo star 400M attached to two slave 400A and software v5.53 ks285 and tried also with v5.53 ks284
I can read the master only, how I can read the two slaves?
This article will help you understand the differences between older S700 (S701-724) drives with single-channel STO and newer dual-channel STO S700 drives.
Abbreviations
Country Codes
Language Codes
Multi Language Terms List
Standards and Directives
Worldwide Electrical Outlet List
Archives/Download
Downloads can be found on the KDN
The command for clearing the fault history on the Servostar S300, S600, and S700 drives is CLREEPROM FLTHIST. That is a space between the two words. Type it into the terminal command line and press enter. Sometimes it is…