New Features
Next Generation Controller Software
Compatible with PCMM/PDMM (1st Generation Controllers)
64-bit Runtime (2nd Generation Controllers)
AKD2G Modular Device Profile (MDP) I/O
MDP IO support for model variants
New…
Hi, i have a project with 3 axes, the web server show one.
What do I have to do to be able to view all the axes on the web server?
KAS version: 3.07.0.88510
Firmware vesion: 3.07.0.88510
AKD firmware version: 01-21-00-000
New Features
Modular EtherCAT Topology
AKT2G-BRC-000-000 - Brake chopper terminal
Modify PLCopen axis user units from a program
IDE Improvements
For more details, please see the attached release note.
New Features
Kollmorgen E-Bus Stepper Integration:
AKT2G-SM-L50-000 - Stepper motor terminal with incremental encoder, 50 V DC, 5 A (Imax), 2 phases
AKT2G-SM-L15-000 - Stepper motor terminal with incremental encoder, 24 V DC, 1.5 A (Imax), 2…
New features include TCP/IP Function Blocks, BBH FSoE Master + SafePLC with KAS-IDE and AKD2G w/ SMM, KAS IDE-WorkBench Improvements, new File Management functions, DriveParamStrRead, Multi-select PDO objects, new axis parameter to read PLCopen…
Hi,
I have a setup where I use the AKD PDMM drives and I would like to know if there is a possibility of using an SSI interface encoder as the feedback device. I know the drives support BiSS-C which is similar to SSI and online resources say…
New Features
FailSafe over EtherCAT (FSoE) "Black Channel" Communication
AKD2G Drive Integration:
Backup/Restore
AKD2G with SMM options #2 (basic) and #3 (advanced)
Robotic Kinematic Transforms: T-Bot, H-Bot, and Gantry
IDE…
I'm using a AKD-M01206 with a direct drive motor. In my KAS-IDE project, I was using X9 as an input to monitor another encoder in the system, but now I want to use it as an output so another system can monitor the motor the AKD is driving.