New features include:
Enhanced AKD2G Drive Integration
Map EtherCAT feedback to PLCopen Digitizing Axis
Multiple IDE Instances
IDE Ease-of-Use Enhancements:
Elastic Search capability in On-Line help
See the article for more information.
Hello,
I want to communicate in PDMM controller via HTTP. Actually I can read from them in C++ but I can't write any value to the variable of PDMM controller in C++. Furthermore I am able to write and read via http with the language of C# by…
The KAS extended template shows the use of different basic functionality, when using the pipe network motion engine. It’s based on the standard two axis pipe network example and includes some of the most common use cases. It covers the following…
The system covered includes a PxMM controller with up to twelve additional AKD drives.
All automation functions are handled in the PLC, the functionality covers the following:
Hello sir,
Is AKD M01206-MCEC suitable for application in which I want to rotate my motor at my required load torque with constant speed?
What are the Inputs & Outputs of the System?
Visão Geral
Para visualizar os alarmes dos drives AKDs na IHM AKI é necessário cadastar todos os alarmes de cada drive no Alarm Server da IHM e inserir código no programa fonte do PLC. Este documento ensina a usar as opção de importação de tabelas e…
Overview
To view the AKDs alarms on the HMI AKI is necessary to register all alarms of each drive in the HMI Alarm Server and insert code in the PLC source program. This document teaches the use of import…
We have a small demo unit consisting of a PDMM and an ethercat AKD. Suddenly the drive is giving a error code of just --. I cannot scan the drive to the ethercat network and can't connect to it from workbench. I'm…