This article will help you understand the differences between older S700 (S701-724) drives with single-channel STO and newer dual-channel STO S700 drives.
The term "dual use" identifies the basic usability of a technology (both a machines and software) as used for both peaceful and military purposes.
For example, drive components used in high-speed centrifuges can be used in both pharmacology and for…
Valid for S300, S700
Most of the ACOMEL drives used in high frequency applications can be replaced with S300/S700 servo amplifiers with special firmware.
Dual Use
These devices are export controlled ( Dual Use, AL-3A225 ) and require an export…