Hall Effect Sensors are used to establish proper motor commutation on Brushless Servo motors. To be effective, the Hall Effect Sensors must be properly aligned with the servo motors phases. Motor manufacturers typically align the Hall…
Hall-ONLY as a Feedback in S300/S700 Drives:
Hall-ONLY as a Feedback has some specific characteristics. This document aims to enhance the comprehension of Hall-ONLY.
Hall-segments:
For any electrical revolution (2 motorpoles) the…
Valid for S300, S400, S600, S700
Incremental encoders with Hall Sensors are a combination of incremental signals for positioning and Hall signals for commutation. The incremental signals can have 5V (TTL) level or 24V level. Encoders with Hall and…